Interfaces Records

This topic provides an alphabetical list and description of the fields that exist for the Interfaces family and appear on the Interfaces datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.

Field

Data Type

Description

Behavior and Usage

Is Default

Logical

Indicates whether the record is the default one. If set true, then the SRS Template is a default template for the category supplied by GE Digital.
Last Modified By Character The name of the user who last modified the record. On the datasheet, this field is disabled and updated automatically whenever the record is modified.
Last Modified Date Date The date on which the record was last modified. On the datasheet, this field is disabled and populated automatically.
Revision Number Numeric A number that represents the number of times the record has been revised. On the datasheet, this field is disabled and populated.
SIF Process Interfaces Text All the interfaces to and from the SIS. On the datasheet, this field appears as a text box, in which you can enter the interfaces (in and out) to and from the SIS.
SIS Sequence of Events Recording Text The sequence of events recording for the events in a SIS. On the datasheet, this field appears as a text box, in which you can enter the SOE design details, typically supplied by the OEM of the SER. (Sequence of events recorder)
SIS to BPCS Interface Details Text The interface to a DCS or BPCS. On the datasheet, this field appears as a text box, in which you can enter the BPCS interface design details.
SIS to Historian Interface Details Text The interfaces to a process historian. On the datasheet, this field appears as a text box, in which you can enter the process historian interface design details.
SRS Template Description Character A description of the record. On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the record.
SRS Template ID Character The ID of the record. On the datasheet, this field appears as a text box labeled Field ID, in which you can type the ID.

Copyright © 2018 General Electric Company. All rights reserved.