Hardware Records

This topic provides an alphabetical list and description of the fields that exist for the Hardware family and appear on the Hardware datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.

Field

Data Type

Description

Behavior and Usage

Inputs Accuracy

Text

This field describes the accuracy of the input hardware. On the datasheet, this field appears as a text box, in which you can enter the input point signal accuracy specifications that the SIS input point is designed to handle.
Inputs Certification Requirements Text This field describes the certifications for the input hardware. On the datasheet, this field appears as a text box, in which you can enter the input point certifications (design basis).
Inputs Response Time Text This field describes the response time of the input hardware. On the datasheet, this field appears as a text box, in which you can enter the input point response time specifications that the SIS input point is designed for.
Inputs Trip Set Points Text This field describes the trip setpoint used for the input hardware. On the datasheet, this field appears as a text box, in which you can enter the input point trip setpoints that the SIS input point is designed to handle.
Is Default Logical Indicates whether the record is the default one. If set true, then the SRS Template is a default template for the category supplied by GE Digital.
Last Modified By Character The name of the user who last modified the record. On the datasheet, this field is disabled and updated automatically whenever the record is modified.
Last Modified Date Date The date on which the record was last modified. On the datasheet, this field is disabled and populated automatically.
Outputs Certification Requirements Text This field describes the certifications of the output hardware. On the datasheet, this field appears as a text box, in which you can enter the design basis for the output point certifications.
Outputs Stroke Times Text This field describes the stroke times of the output hardware. On the datasheet, this field appears as a text box, in which you can enter the design basis for the output point stroke times.
Outputs leakage requirements Text This field describes the leakage requirements of the output hardware. On the datasheet, this field appears as a text box, in which you can enter the design basis for the output point leakage requirements.
Revision Number Numeric A number that represents the number of times the record has been revised. On the datasheet, this field is disabled and populated.
SIS Input (sensor) Module Requirements Text This field describes the requirements for the input hardware module. On the datasheet, this field appears as a text box, in which you can enter the input module design basis, typically supplied by the OEM of the input module.
SIS Logic Solver Requirements Text This field describes the requirements for the logic solver hardware module. On the datasheet, this field appears as a text box, in which you can enter the logic solver design basis, typically supplied by the OEM of the input module.
SIS Output (final element) Module Requirements Text This field describes the requirements for the output hardware module. On the datasheet, this field appears as a text box, in which you can enter the output module design basis, typically supplied by the OEM of the input module.
SRS Template Description Character A description of the record. On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the record.
SRS Template ID Character The ID of the record. On the datasheet, this field appears as a text box labeled Field ID, in which you can type the ID.

Copyright © 2018 General Electric Company. All rights reserved.