This topic provides an alphabetical list and description of the fields that exist for the Environment family and appear on the Environment datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Is Default |
Logical |
Indicates whether the record is the default one. |
If set true, then the SRS Template is a default template for the category supplied by GE Digital. |
Last Modified By | Character | The name of the user who last modified the record. | On the datasheet, this field is disabled and updated automatically whenever the record is modified. |
Last Modified Date | Date | The date on which the record was last modified. | On the datasheet, this field is disabled and populated automatically. |
Revision Number | Numeric | A number that represents the number of times the record has been revised. | On the datasheet, this field is disabled and populated. |
SIS Environment - Electrical Classification | Text | Describes if the SIS is approved for hazardous area. CSA, FM, ATEX and IECx certification will be described here. Also, electrical housing holding the SIS will be described here. | On the datasheet, this field appears as a text box, in which you can enter the hazardour area approval details. |
SIS Environment - Humidity | Text | The relative humidity specification for the SIS control system will be described here. (for example, 5 to 95% non-condensing) | On the datasheet, this field appears as a text box, in which you can enter the relative humidity specifications that the SIS is designed to handle. |
SIS Environment-Temperature | Text | The operating temperature range and the storage temperature range will be described here. (for example, -40 to 70 C operating temperature range and -40 to 85 C storage temperature range). | On the datasheet, this field appears as a text box, in which you can enter the operating temperature range specifications and storage temperature specification range that the SIS is designed to handle. |
SIS Environmental Conditions | Text | The environmental fields describes the airborne contaminants, shock and vibration conditions. (for example, airborne contaminants: ISA-S71.04-1985 Airborne Contaminants Class G3 Conformal coating, shock: 10 g ½-sine wave for 11 ms and vibration: 1 mm peak-to-peak from 2 to 13.2 Hz) | On the datasheet, this field appears as a text box, in which you can enter the environmental specifications that the SIS is designed to handle. |
SRS Template Description | Character | A description of the record. | On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the record. |
SRS Template ID | Character | The ID of the record. | On the datasheet, this field appears as a text box labeled Field ID, in which you can type the ID. |
Copyright © 2018 General Electric Company. All rights reserved.