This topic provides an alphabetical list and description of the fields that exist for the Electrical family and appear on the Electrical datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
I/O Power Redundancy Requirements |
Text |
Describes if redundant power supplies are feeding power to the SIS. |
On the datasheet, this field appears as a text box, in which you can enter a true or false and then the description of the redundancy (dual or triple redundant). |
I/O Power Requirements | Text | I/O power provided for the SIS. | On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the I/O power provided (for example: 24V DC) |
I/O Power Sources | Text | The source of the I/O power (for example, clean power from a UPS, batter power, etc) | On the datasheet, this field appears as a text box, in which you can enter a true or false and then the description of the source (for example: from UPS A, or battery bank B) |
Is Default | Logical | Indicates whether the record is the default one. | If set true, then the SRS Template is a default template for the category supplied by GE Digital. |
Last Modified By | Character | The name of the user who last modified the record. | On the datasheet, this field is disabled and updated automatically whenever the record is modified. |
Last Modified Date | Date | The date on which the record was last modified. | On the datasheet, this field is disabled and populated automatically. |
Loss of SIS Energy Sources | Text | The consequences, if one or more SIS energy (power) sources are disabled. | On the datasheet, this field appears as a text box, in which you can enter the description of consequence if one more sources is disabled. |
Revision Number | Numeric | A number that represents the number of times the record has been revised. | On the datasheet, this field is disabled and populated. |
SRS Template Description | Character | A description of the record. | On the datasheet, this field appears as a text box labeled Description, in which you can enter a description of the record. |
SRS Template ID | Character | The ID of the record. | On the datasheet, this field appears as a text box labeled Field ID, in which you can type the ID. |
Copyright © 2018 General Electric Company. All rights reserved.