SIS Proof Test Template Detail Records

This topic provides a list of the fields that exist in the SIS Proof Test Template Detail family. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Comments Character Comments about the proof test.

This field does not appear in the Proof Test Template datasheet. However, it appears in the Functional Test Detail datasheet when you link this Proof Test Template to a Proof Test. This field also appears when you print the Proof Test Template.

Equipment ID

Character

The ID of the Equipment against which the step should be performed.

You can select the associated Equipment by selecting the in the Equipment ID field.

Location ID Character The ID of the Functional Location against which the step should be performed. You can select the associated Functional Location by selecting the Location ID field.
Result Criteria Text A description of what is considered to be an acceptable result of the step. None
Step Sequence Number Number A number that represents the order in which the step should be performed, relative to other steps. When you create a new SIS Proof Test Template Detail this value is set automatically based upon the values in existing SIS Proof Test Template Details. You can modify this value manually in both new and existing records.
Step Type Character The type of step.

On the datasheet, you can select the step type from a list of the following options:

  • Pretest Setup
  • Sensor
  • Logic Solver
  • Final Element
  • Post Test Procedure
Template Detail ID Character An alphanumeric value that identifies the SIS Proof Test Template Detail.

This field is populated with a default value appended with the step number and the step type. You can modify this value if required. This value must be unique.

Travel Time Limit Number A number that quantifies the maximum acceptable travel time for this step, in seconds. This field is enabled only in SIS Proof Test Template Details where the step type is Final Element.
Trip Point Number A number that defines when the element will activate an SIS shutdown. This field is enabled only in SIS Proof Test Template Details where the step type is either Sensor, Final Element, or Logic Solver.
Trip Point Direction Character The trend of Trip Point values. This field is enabled only in SIS Proof Test Template Details where the step type is either Sensor, Final Element, or Logic Solver.
Trip Point Error Limit Number A value that defines the range, plus or minus, within which the Trip Point value must fall to be acceptable. This field is enabled only in SIS Proof Test Template Details where the step type is either Sensor, Final Element, or Logic Solver.
Trip Point Units Character The unit of measure associated with the value in the Trip Point field. This field is populated with a list of System Codes that exist in the UOME system code table. This field is enabled only in SIS Proof Test Template Details where the step type is either Sensor, Final Element, or Logic Solver.

Copyright © 2018 General Electric Company. All rights reserved.