SIL Threshold Records

SIL Threshold records store information about the numeric range for risk value for each Safety Integrity level, and are used when assessing SIL value using Risk Matrix or PHA. This topic provides an alphabetical list and description of the fields that exist for the SIL Thresholdfamily. The information in the table reflects the baseline state and behavior of these fields.

IMPORTANT: The records in this family can be modified only by users who belong to the Security Groups MI SIS Administrator.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Lower Boundary Numeric The lower boundary value of risk rank for the SIL value identified in the SIL level field. You can enter a value manually.
Mitigated Risk Factor Numeric A number indicating the tolerable risk probability for an Instrumented Function.

You can enter a value greater than 0 and less than or equal to 1.

The value in this field is divided by the Driving Risk Rank value in the Risk Matrix of the SIL Assessment to determine the Required Probability of Failure.

If this field is blank, a default value of 1 will be used in the calculation.

SIL Level Numeric The Safety Integrity Level for which the unmitigated risk range is defined. You can enter a value manually.
Upper Boundary Numeric The upper boundary value of risk rank for the SIL value identified in the SIL level field. You can enter a value manually.

Copyright © 2018 General Electric Company. All rights reserved.