The required probability of failure is a number representing the probability that an instrumented function will fail in a dangerous scenario. This value is represented as a probability value (e.g., .001), and is an indicator of whether the instrumented function is meeting its requirements to mitigate risk. The required probability of failure value is based on the following values stored in the Instrumented Function:
The following sections describe how the required probability of failure is calculated based on the SIL value, assessment method, and demand rate.
Copyright © 2018 General Electric Company. All rights reserved.