Protective Instrument Loop Final Element System records store details about a protective instrument loop final element system that you have created as part of SIL verification. This topic provides an alphabetical list and description of the fields that exist for the Protective Instrument Loop Final Element System family and appear on the Protective Instrument Loop datasheet by default. The information in this table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Availability | Number | A number representing the percentage of time between proof tests that the final element system is expected to be available. |
The GE Digital APM system calculates this value using the following calculation: Availability = (1 - PFD) * 100 |
Calculated PFD Avg | Number | A number representing the probability that the final element system will fail to react during a demand when the loop is operating in a low demand mode. | This field is disabled. The GE Digital APM system calculates and populates this value. This value depends on the failure rate of the final element system. |
Calculated PFH | Number | A number representing the probability that the final element system will fail to react during a demand when the loop is operating in high demand or continuous mode of operation. | This field is disabled. TheGE Digital APM system calculates and populates this value. This value depends on the failure rate of the final element system. |
Calculated STR | Number | A number representing the spurious trip rate for the logic solver. | This field is disabled. The GE Digital APM system calculates and populates this value. |
Common Cause (Beta) | Number | A number representing the percentage of failure that would affect the functioning of multiple devices. For example, a power supply failure for a final element system that is shared across multiple loops can cause all the loops to fail. In this case, the beta factor is the probability that the loops fail in case of a power supply failure to the final element system. |
If the value in the Voting field is 1oo1 or 1001D, this value is not applicable. This value is populated automatically when you select a device. |
HFT | Number | A number representing the hardware fault tolerance, or the number of failures the final element system can tolerate before failing. | For example, a final element system with 1oo2 redundancy has a HFT of 1 because it can tolerate one failure and can still continue to operate. |
MTTFS | Number | A number representing Mean Time To Fail Spuriously for a Final Element. For example, suppose a final element system senses a hazard that does not exist. In this case, MTTFS is the expected time that the process fails spuriously. | This field is disabled. The GE Digital APM system calculates and populates this value. |
Number of Groups | Number | The number of final element groups in the system. | This field is disabled and populated with the number of final element groups in the system. |
SIL Architectural Constraints | Number | A number that represents the SIL value for the final element system, which is based on the architectural constraints that are defined in the Test Architecture Constraints field. | This field is disabled. The GE Digital APM system calculates and populates this value. |
SIL Systematic Capability | Number | A number that represents the SIL value for the final element system, which is based on the systematic capability that is defined in the Test Architecture Constraints field. | This field is disabled. The GE Digital APM system calculates and populates this value. |
System ID | Character | The ID of the final element system. | This value is required and is populated with a default value. You can, however, provide a different value. |
Voting Between Groups | Character | The voting architecture that represents the minimum number of final element groups that should trip (in the event of a failure) and the number of final element groups available in the system. For example, if the voting is 1oo2, then for the logic solver to detect a failure, at least one final element group should trip out of the two final element groups that are available in the group. |
This field is updated automatically when you add or remove a final element group from the system. The following options are available:
This value is required. |
Copyright © 2018 General Electric Company. All rights reserved.