SIS Proof Test Task records store details about an inspection task of the type proof test. This topic provides an alphabetical list and description of the fields that exist for the SIS Proof Test family and appear on the SIS Proof Test datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Coverage | Number | A number that indicates how confident you are that the proof test will be able to detect failures. | Enter a value between 0 and 100. |
Desired Interval | Number | A number indicating how often the task should be completed. |
This number must be between the Min Interval and Max Interval values. Before you can save a value in this field, the Last Date field must contain a value. The next date is calculated automatically using both the last date and desired interval. The units that you select for the desired interval are also applicable to the Max Interval and Min Interval. |
Desired Interval Basis | Character | The basis on which you have specified the desired interval. | None |
Last Date | Date | The date on which the associated Proof Test Event is closed. |
By default, this field contains the date on which the Proof Test Task is created. After you close the Proof Test Event linked to this Proof Test Task, this field is disabled and populated with the date on which the Proof Test Event is closed. This value is also populated in the Date Executed field in the Task Execution record that is linked to this Proof Test Task. |
Max Date | Date | The latest date by when you must perform the task. |
This field is disabled and calculated as follows: Max Date = Last Date + Max Interval |
Max Interval | Number |
The maximum interval to perform the task. For example, if the value in this field is 30 days, it implies that you must perform the task within 30 days from the day you last performed the task. |
None |
Min Date | Date | The earliest date on which you can perform the task. |
This field is disabled and calculated as follows: Min Date = Last Date + Min Interval |
Min Interval | Number |
The minimum interval to perform the task. For example, if the value in this field is 15 days, it implies that you must perform the task after 15 days from the day you last performed this task. |
None |
Modifiable | Logical | Indicates whether the Task can be modified. | This check box is selected automatically when you create a Proof Test Task and cleared after you save the record. |
Next Date | Date |
The suggested date by when you must perform the task. For example, if the value in this field is 20 days, it is suggested that you perform the proof test task after 20 days from the day you last performed this task. |
This field is disabled and calculated as follows: Next Date = Last Date + Desired Interval |
Next Date Basis | Character | The basis on which you have specified the next date for performing the task. | None |
Override Interval | Logical | Indicates whether you can override the value in the Desired Interval field. | If you select this check box, you can modify the value in the Desired Interval field. |
Rejectable | Logical | Indicates whether the task can be rejected. | If you clear this check box, you will not be able to reject the task. |
Character | The ID of the Asset that is linked to the task. | None | |
Reoccurring | Logical | Indicates whether the task is recurring. | None |
Source Type | Character | The type of the source for the proof test (e.g., Hazards Analysis, SIS, FMEA). | None |
Task Assigned To | Character | The name of the person who has been assigned the task. | None |
Task Description | Character | A description for the task. | None |
Task Details | Character | The details of the task. | None |
Task ID | Character | The ID for the task. | This field must be unique. |
Task State | Character | The state associated with the Calibration Task. By default this field contains the value Proposed. | This field contains a list of states. After you save a new Calibration Task, this value is changed automatically from Proposed to Scheduled without change. |
Task Type | Character | The type of task. |
This field appears contains a list of values from the Task Type family that correspond to types of calibrations (e.g., CALIBRATION: AUTOMATED, ANALOG, 11 UP/DN, LINEAR, DCV/DCV). You must select the value PROOF TEST. |
Unconstrain Min/Max Dates | Logical | Indicates whether you can override the next date. |
When you select this check box, the values in the Min Date and Max Date fields are cleared. |
Copyright © 2018 General Electric Company. All rights reserved.