Logic Solver records store details about the safety instrumented system that they represent. This topic provides an alphabetical list and description of the fields that exist for the Logic Solver family. Unless otherwise specified, the fields appear on the Logic Solver datasheet. The information in this table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Abnormal Mode Description | Text | A detailed description of the abnormal mode of operation. | This field is enabled only if Abnormal is selected in the Plant Operation Mode list. Otherwise, this field is disabled. |
Abnormal State | Character | A short description of the specific abnormal state of the operation. | This field contains a list with
the following values:
|
Communication Links | Character | The type of communication link that exists between components within the logic solver and any other network device (e.g., Ethernet). | None |
Is Default SIS | Logical | Indicates whether the Logic Solver is the default one. | This field does not appear on the datasheet by default. |
Last Modified By | Character | The name of the user who last modified the record. | On the datasheet, this field is disabled and updated automatically whenever the record is modified. |
Last Modified Date | Date | The date on which the record was last modified. | On the datasheet, this field is disabled and populated automatically. |
Logic Solver ID | Character | The ID for the logic solver that is associated with the safety instrumented system. | This value should correspond to the value stored in the Logic Solver ID field in the Protective Instrument Loop Logic Solver that represents the desired logic solver. |
Logic Solver Type | Character | The type of logic solver. | This field contains
the following baseline System Codes in the MI LOGIC SOLVER TYPE System Code Table:
|
Long Description | Text | A statement describing the purpose of the safety instrumented system. | None |
Manual Shutdown Description | Text | A description of the method by which the safety instrumented system can be manually shut down. | None |
Mission Time | Number | A numeric value (in years) that represents the time that the safety instrumented system will be in use before it is replaced or remanufactured. | On the datasheet, this field appears as a text box labeled Mission Time with an additional label, Years, to the right of the text box. You can enter your own value, which should be equal to or greater than the length of time specified in the Target SIS Test Interval field. |
Operation Mode | Character | The mode of operation for the safety instrumented system. | On the datasheet, this field appears as a list labeled Plant Operation Mode and contains
the following values:
|
Plant ID | Character | The ID of the plant in which the safety instrumented system exists. | By default, this field does not appear on the datasheet. |
Plant Operation Mode | Character | The operational mode of the process for which the logic solver is expected to operate. | This field contains a list with following values:
|
Power Source | Character | A description of the power supply to the safety instrumented system. | None |
Remove Default | Logical | Allows you to remove the default logic solver settings. | After you remove the default logic solver settings:
|
Reset Procedure | Text | A description of the method by which the safety instrumented system can be reset. | None |
Set as Default | Logical | Allows you to set the selected logic solver as default. | After you set a logic solver as default:
Note: If the selected logic solver is already set as default, the Remove Default button is displayed instead of the Set as Default button. |
SIS Description | Character | A description for the safety instrumented system. | None |
SIS ID | Character | A name for the safety instrumented system. | This field is required, and must be unique. If the value that you enter is already specified for an existing Logic Solver, a message will appear, indicating that the value is already in use. You will need to specify a different value before you can save the record. |
Site Description | Character | A description of the site that is specified in the Site ID field. | This field does not appear on the datasheet by default. |
Site ID | Character | The ID of the Site that is associated with the safety instrumented system. | On the datasheet, this field is disabled and populated automatically with the value stored in the Site ID field in the associated SIL Analysis. You should not modify this value. |
Target SIS Test Interval | Number | A number that represents the interval in months by which regular testing will be performed on the safety instrumented system. | None |
Unit Description | Character | A description of the unit specified in the Unit ID field. | This field does not appear on the datasheet by default. |
Unit ID | Character | A description of the area in which the safety instrumented system exists. | None |
Copyright © 2018 General Electric Company. All rights reserved.