Queries Folder

The Catalog folder \\Public\Meridium\Modules\Risk Based Inspection\Queries contains the following items.

Query Name Behavior and Usage
Active Analyses for Evergreening - 580

Returns the RBI Criticality Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the active state.
  • Have an evergreening Batch ID.
Active Analyses for Evergreening - 581

Returns the RBI 581 Risk Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the active state.
  • Have an evergreening Batch ID.
Analyses Created For Evergreening - 580

Returns the RBI Criticality Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the Created state.
  • Have an evergreening Batch ID.

IMPORTANT: Do not modify the following columns: Analysis ID, Component, Asset ID, Analysis Entity Key, and Risk Category. Modifying these columns may affect the Calculate functionality during the evergreening process.

Analyses Created For Evergreening - 581

Returns the RBI 581 Risk Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the Created state.
  • Have an evergreening Batch ID.

IMPORTANT: Do not modify the following columns: Analysis ID, Component, Asset ID, Analysis Entity Key, and Risk Category. Modifying these columns may affect the Calculate functionality during the evergreening process.

Analyses Ready for Evergreening - 580

Returns the RBI Criticality Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the active state.
  • Have not been evergreened.
  • Have not been calculated in the last five years.

IMPORTANT: Do not modify the ENTY_KEY column. Modifying this column may affect the duplicate functionality during the evergreening process.

Analyses Ready for Evergreening -581

Returns the RBI 581 Risk Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the active state.
  • Have not been evergreened.
  • Have not been calculated in the last five years.

IMPORTANT: Do not modify the ENTY_KEY column. Modifying this column may affect the duplicate functionality during the evergreening process.

Analyses Ready for Evergreening for Unit - 580

Returns the RBI Criticality Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the active state.
  • Have not been evergreened.

IMPORTANT: Do not modify the ENTY_KEY column. Modifying this column may affect the duplicate functionality during the evergreening process.

Analyses Ready for Evergreening for Unit - 581

Returns the RBI 581 Risk Analysis records for RBI Components linked to RBI Assets that:

  • Are related to the given Functional Location or Process Unit key.
  • Are in the active state.
  • Have not been evergreened.

IMPORTANT: Do not modify the ENTY_KEY column. Modifying this column may affect the duplicate functionality during the evergreening process.

Asset Corrosion Analysis More Current Than Analyses

Returns all Assets linked to a Functional Location that have a TM Asset Corrosion Analysis more current than the active RBI analysis on the component.

Note: This query will not return RBI 581 analyses.

Asset Counts for Units Returns a count of assets that contain RBI data that is linked to Functional Locations hierarchically.
Assets with No Recommendations

Returns all assets linked to a Functional Location that do not have any Recommendations and at least one component with a risk complete analysis without RBI Recommendations.

IMPORTANT: Do not modify the Asset Entity Key field. Modifying this field may affect the generate recommendation functionality.

Criticality Consequence Evaluation None
Current Risk Returns the current rolled-up risk for each Asset under a Functional Location.
Current Risk Overview Returns the highest Risk Category for each Asset under a Functional Location and gives a count.
Export RBI Components by Asset Returns Equipment records that are linked to Active RBI Components and Equipment records that are not linked to at least one RBI Component.
Inspections More Current Than Analysis

Returns all Assets linked to a Functional Location that have Inspections more current than the active RBI analysis on the component.

Note: This query will not return RBI 581 analyses.

Invalid Inspections for Non-Intrusive Requirement Met None
Manage Inspection Groups None
Manage RBI Components None
Manage RBI System None
Maximum Internal Corrosion Rate Returns the calculated maximum internal corrosion rate for an Internal Corrosion DME.
Past Risk Returns the past rolled up risk for each Asset under a Functional Location.
Past Risk Overview Returns the highest Risk Category for each Asset Under a Functional Location and gives a count.
PRD Consequence Evaluation None
Process Unit Query Returns a list of the Process Units that fall under the selected level of the Asset Hierarchy. Also returns a count of assets that are related to each given Process Unit hierarchically.
RBI Asset Risk Query None
RBI Asset Risk Sub Query None
RBI Assets for a Functional Location Returns all Assets linked to a Functional Location.
RBI Components for an Asset Returns all RBI Components for a given Asset.
RBI Corrosion Loops for a Functional Location Returns all Corrosion Loops linked to a given Functional Location.
RBI DM Query None
RBI Flexible Configuration Records Returns all custom Degradation Mechanism Evaluation Configuration records.
RBI Flexible Validation Records Returns all custom Degradation mechanism Evaluation Validation records.
RBI Overview Filter Parameters None
RBI Pipeline Consequence Evaluation None
Recommendations by Asset Returns RBI Recommendation records related to the selected asset.
Review Analyses by Asset 580 Return all RBI Criticality Analysis records that are calculated in Created state for the Equipment or Functional Location record for which you accessed the RBI Asset.
Review Analysis by Corrosion Loop 580 Return all RBI Criticality Analysis records that are calculated in the Created state for the Corrosion Loop record for which you accessed the RBI Asset.
Review Analyses by Asset 581 Return all RBI 581 Risk Analysis records that are calculated in the Created state for the Equipment or Functional Location record for which you accessed the RBI Asset.
Review Analysis by Corrosion Loop 581 Return all RBI 581 Risk Analysis records that are calculated in Created state for the Corrosion Loop record for which you accessed the RBI Asset.
Select Protected Assets Return Equipment records on the Select Protected Equipment window.
Select Protected RBI Components Returns RBI Components on the Select Protected Equipment window.
Select RBI Components

Returns RBI Components that are:

  • Linked to Equipment records.
  • Not linked to a Corrosion Loop record.
Select Unit for Grouping

Returns all Functional Location records that:

  • Represent a unit.
  • Are linked to an Corrosion Loop record that is associated with RBI Components.
Unlinked Corrosion Loops Returns all Corrosion Loops that are not linked to a Unit.
Valid Inspections for Non-Intrusive Requirement Met None
View all Recommendations Returns all recommendations for a selected Unit.
View Protected RBI Components Returns all Protected RBI Components for a selected Unit.
Policy Queries folder Contains queries that are used by RBI Strategy Mapping Groups when you generate RBI Recommendations records automatically.

Copyright © 2018 General Electric Company. All rights reserved.