Records in the PV Stress family make up the PV Stress reference table, which GE Digital APM uses to locate the appropriate Allowable Stress value for RBI
This topic provides an alphabetical list and description of the fields that exist in the PV Stress family. The information in the table reflects the baseline state and behavior of these fields. The Material Type, Minimum Tensile Strength, and Minimum Tensile Yield fields exist in the PV Stress family, but they are not used to determine the Allowable Stress value.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Allowable Stress | Numeric | The maximum amount of pressure that can safely be withstood by a component. |
This value in this field, in addition to the following other PV Stress fields,
is used to determine the value that is populated in the Allowable Stress field in
the associated RBI
|
Code Year | Character | The year in which the design code that corresponds to the component was defined. |
The value in this field is used to populate the Code Year field in the associated RBI This field must contain a value in order for GE Digital APM to retrieve:
|
Design Code | Character | The design code associated with the component. |
The value in this field is used to populate the Construction Code field in the associated
RBI This field must contain a value in order for GE Digital APM to retrieve the value in the Allowable Stress field in the PV Stress record from the PV Stress Reference table. |
Material Grade | Character | The material grade of the component. |
The value in this field is used to populate the Material Grade field in the associated
RBI This field must contain a value in order for GE Digital APM to retrieve the value in the Allowable Stress field in the PV Stress record from the PV Stress Reference table. |
Material Specification | Character | The material specification of the component. |
The value in this field is used to populate the Material Spec field in the associated
RBI This field must contain a value in order for GE Digital APM to retrieve:
|
Metal Temperature | Numeric | The temperature of the metal of which the component is made. |
The value in this field is used to populate the Design Temperature field in the associated
RBI This field must contain a value in order for GE Digital APM to retrieve the value in the Allowable Stress field in the PV Stress record from the PV Stress reference table. |
Minimum Tensile Strength | Numeric | The minimum tensile strength of the material of the component. | None |
Minimum Yield Strength | Numeric | The minimum yield strength of the material of the component. | None |
Copyright © 2018 General Electric Company. All rights reserved.