For each Mitigated Risk that is associated with the Special Action, you can specify the Failure Consequence values that you want to be used in the simulation when the Special Action is completed to mitigate the occurrence of the given Risk.
Steps
In the New Failure Consequence column, select the hyperlink.
The Failure Consequence window appears.
In the lower-left corner, select the Replace Failure Consequence check box.
The fields in the Failure Consequence window are enabled.
Select OK.
The changes are saved, and the values that you specified will be used the next time the simulation is run.
Copyright © 2018 General Electric Company. All rights reserved.