Remove a Resource Assigned to a Risk

When you remove a Resource from a Risk, you delete the System Resource Usage record so that the Resource is no longer used by the selected Risk. The actual System Resource record is still available for the System Reliability Analysis and can be used if needed.

Steps

  1. Access the Risk to which you want to modify a resource.
  2. In the grid, locate the row containing the Risk for which you want to modify a Resource.

  3. If you want to remove a planned Resource, select the Planned Resource Usages link.

    -or-

    If you want to remove an unplanned Resource, select the Unplanned Resource Usages link.

    The <Risk> - <Resource Usage> grid appears, displaying the list of resources that are assigned to the selected Risk. <Risk> is the name of the Risk that you selected and <Resource Usages> is the type of Resource Usage that you selected.

    The following image shows the grid when you select Unplanned Resource Usage:

    Unplanned Resource Usage

  4. In the grid, select the row containing the resource that you want to remove, and then select .

    A message appears, you to confirm that you want to remove the selected Resource.

  5. Select OK.

    The Resource is removed from the grid, and the System Resource Usage record is deleted from the database.

Copyright © 2018 General Electric Company. All rights reserved.