System Special Action Records

System Special Action records store information about procedural, redesign, or training Actions. The following table provides an alphabetical list and description of the fields that exist for the System Special Action family and appear by default on the System Special Action datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Caption Data Type Description Behavior and Usage
Action Cost Number A numeric value that specifies the cost associated with any materials or personnel needed to complete the Action.

This value represents an expense that is incurred every time the Action occurs. By default, this value is set to 0 (zero).

This field is available in the General section of the Properties pane.

Action Type Character The category into which the Action can be classified.

You can select a value from the following options when you create the System Special Action record:

  • Procedure (PROC)
  • Redesign (DSN)
  • Training (TRN)

After you create an Action, this field is disabled.

This field is available in the General section of the Properties pane.

Description Text A text field that stores any additional information about the Action.

You can define this value manually by entering text in the Description box.

This field is available in the General section of the Properties pane.

Duration Number

A numeric value that, combined with the value in the Duration Units field, identifies the total time nedeed to complete the Action.

For example, if the value in the Duration field is 4 and the value in the Duration Units field is Hours, then the Action will take four hours to complete.

By default, this value is set to 0 (zero).

This field is available in the Special section of the Properties pane.

Duration Units Character The time units associated with the value in the Duration field.

You can select a value from the following options:

  • Minutes
  • Hours
  • Days
  • Weeks
  • Months
  • Years

By default, this value is set to Days. This field is available in the Special section of the Properties pane.

GUID Character A value that uniquely identifies the record within a System Reliability Analysis. This value is generated automatically by the GE Digital APM system and does not appear on the System Special Action datasheet. In System Reliability Analyses, GUIDs are used to identify records because Entity Keys will not exist until a record is saved. Because a System Reliability Analysis may contain unsaved records, it is necessary to use a value that uniquely identifies those records within the system.
Interval Number

A numeric value that, combined with the value in the Interval Units field, indicates how often the Action will occur.

For example, if the value in the Interval field is 4 and the value in the Interval Units field is Months, then the Action will occur every four months during the simulation period.

By default, this value is set to 1.

This field is available in the Special section of the Properties pane.

Interval Units Character The time units associated with the value in the Interval field.

You can select a value from the following options:

  • Minutes
  • Hours
  • Days
  • Weeks
  • Months
  • Years

By default, this value is set to Days. This field is available in the Special section of the Properties pane.

Name Character The name of the Action.

You can define this field manually. This value is used to identify Actions in the System Reliability Analyses. For instance, the Name column appears by default in the Actions tab in the workspace and displays values that exist in the Name field to identify the System Action records that are displayed in the workspace.

This field is available in the General section of the Properties pane.

One Time Action Logical Indicates whether the Action will occur one time or will be repeated more than once.

If this check box is selected, the Action will occur once. If this check box is cleared, the Action will occur more than once.

For example, an Action to inspect the vibration level of a pump might occur several times a year. In this case, the One Time Action check box of the corresponding System Special Action record would be cleared. An Action to inspect a newly installed pump for any installation errors might occur only once, in which case the One Time Action check box of the corresponding System Special Action record would be selected. By default, this check box is selected.

This field is available in the Special section of the Properties pane.

Shutdown Required Logical Indicates whether the Action requires the piece of equipment or location to be shut down in order for the Action to be completed.

If this check box is selected, the piece of equipment or location must be shut down in order for the Action to be completed. If this check box is cleared, the Action can be completed while the piece of equipment or location is running.

For example, an Action to inspect the vibration level of a pump could be completed while the pump is running, so the Shutdown Required check box would be cleared. An Action to inspect the internal components of a pump would be completed while the pump is not running, so the Shutdown Required check box would be selected. By default, this check box is selected.

This field is available in the Special section of the Properties pane.

Copyright © 2018 General Electric Company. All rights reserved.