A Spare Application record stores information about age data for the equipment that contains the spare part that you are analyzing. The following table provides an alphabetical list and description of the fields that exist for the Spare Application Population family and appear in the grid by default.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Age | Number | The operational age of the population of equipment that is associated with the data in the linked Spare Application record and Spare record. Age value is the amount of time that the population has been in use. | You can enter a value manually to define this value. |
Age Time Unit | Character | The unit of measure associated with the Age. | The Age Time Unit list is set to Years by default. |
Name | Character | The name of the Spare Application record. |
This is a required field. The name of each Spare Application must be unique to the root record. |
Population Size | Number | The number of pieces of equipment that share the same age. | You can enter a value manually to define this value. |
Copyright © 2018 General Electric Company. All rights reserved.