The Assets section provides following information for each piece of equipment belonging to a Reliability Distribution Analysis:
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field Caption | Data Type | Description | Behavior and Usage |
---|---|---|---|
Asset ID | Character | The ID of the piece of equipment that failed. This is a required field. | You can enter the ID manually. |
Datasheet | Character | A link that displays the datasheet associated with the failure event. | This column appears only when a query is the data source for the analysis. |
Future Age | Numeric | The future age of the piece of equipment. | The value for this field is calculated by the GE Digital APM system by adding the specified operating time to the current age of the piece of equipment and is read-only. |
Future Failure Probability | Numeric | The future probability of equipment failure. | The value for this field is calculated by the GE Digital APM system using the specified operating time and is read-only. You can specify the future time to calculate the future probability of failure. |
Installation Date | Date | The date on which the piece of equipment was installed. | You can enter or select a date. |
Last Replacement Date | Date | The last date on which the failed piece of equipment was replaced. |
The value for this field is calculated by the GE Digital APM system and is read-only. This field does not appear in the grid. |
Number of Subcomponents | Numeric | The number of subcomponents contained by the piece of equipment that is selected in the Asset ID column. A piece of equipment can contain multiple subcomponents, such as tubes in a heat exchanger bundle. | This field is displayed in the grid only when the failure type is Failures Without Replacements. |
Present Age | Numeric | The current age of the piece of equipment. | The value for this field is calculated by the GE Digital APM system and is read-only. |
Present Failure Probability | Numeric | The current probability of failure for each piece of equipment. | The value for this field is calculated by the GE Digital APM system based on the present age of the piece of equipment and is read-only. |
Copyright © 2018 General Electric Company. All rights reserved.