When a rule is executed, only the potential analyses that contain the minimum number of failure points for an analysis will be created or updated. The following number of failure points is required for each analysis that can be created from a Reliability Automation Rule.
If the potential analysis does not contain the corresponding number of failures or more, when the rule is executed, the analysis will not be created.
Note: Before you use a rule to create an analysis, you should review the data required for the type of analysis you are creating. If you use invalid data, the analysis will still be created, but the results will not be valid.
Steps
On the Automation page, in the upper-right corner, select Execute Rule.
The status of the rule execution appears below the Execute Rule button, indicating the progress of execution in percentage.
Note: You can select
The system executes the rule(s) and generates the resulting analyses.
Tip: At the bottom of the page, you can view the Information related to the selected Automation Rule.
Copyright © 2018 General Electric Company. All rights reserved.