If you record event-based data, such as failure dates (e.g., a failure was recorded on 5/5/12), you can create a Reliability Growth Analysis using event-based data and data containing dates.
Note: A minimum of three failure datapoints are necessary to perform a calculation.
Steps
In the upper-right corner of the page, select New Analysis, and then select Reliability Growth.
The Reliability Growth Builder window appears.
Note: All required information is provided, but for additional information, consult the Reliability Growth and Measurement Data topics.
Enter values in the Analysis Name and Description boxes for the new analysis, and then select Next.
The Select Data Source Type screen appears. The Data will be based on an existing Query is selected by default.
If you want to load data using an existing query, select Data will be based on an existing Query, and then select Next.
The Select Query screen appears.
-or-
If you want to load data using an existing dataset, select Data will be based on an existing Dataset, and then select Next.
The Select Dataset screen appears.
Select Browse to search for an existing query or dataset in the GE Digital APM Catalog.
The Query Browser or Dataset Browser screen appears, depending on whether you selected Data will be based on an existing Query or Data will be based on an existing Dataset in the previous step.
The following image shows the screen to select a query:
Select the needed query or dataset from the Catalog, and then select Open.
The complete path to the query or dataset is displayed in the Query or Dataset box. The fields that exist for the selected query or dataset appear in the Available Fields list.
The following image shows the path to a selected query and the fields in the Available Fields list:
In the Includes Data From the Following Sites list, select the site(s) whose data from which you want to create an analysis.
Note: If you are creating an analysis in a database that has only one site stored in the Site Reference family, then the Includes Data From the Following Sites list will not appear on the Select Query screen.
Select Next.
The Select Data Format screen appears.
On the Select Data Format screen, specify the following:
In the Measurement Data Format section:
If you want to use the datasource with data that contains event counts, such as number of equipment failures, safety incidents, or equipment repairs, select Data is event count (e.g. Number of failures).
-or-
If you want to use the datasource with data that does not contain event counts but contains an amount, such as cost or hours, select Data is not event count (e.g. Costs).
Note: These instructions assume that you will select Data is event count, and leave the Measurement Name box with the default value Failures.
Select Next.
The Select Data Fields screen appears.
Select the columns from your query or dataset that you want to map to the Reliability Growth Analysis. The available columns are:
Select Next.
The Provide Information for Downtime screen appears.
In the Time Unit list, select the time units associated with the selected downtime from the following options:
The default value is Days.
Select Finish.
The GE Digital APM system generates the analysis and the Reliability Growth page appears, displaying the analysis results.
Copyright © 2018 General Electric Company. All rights reserved.