To create a Probability Distribution Analysis, you must select the field that contains the value that you want to analyze.
The following table shows the typical data needed to build and analyze Probability Distribution Analyses.
Data Required | Data Type | Description | Behavior and Usage |
---|---|---|---|
Censored |
Logical |
As needed, select the field to provide censoring information. Select the field from the data source that contains a value that indicates censored values. |
This field is optional. |
Random Variable |
Character |
If the data source is a query, the name of the random variable and the units of measure will be pre-populated based on the selection you made in the Value field on the previous screen. If you selected a different data source, type the name of the random variable in the Random Variable field and the units of measure for the random variable in the Units field. |
This field is optional.
|
Units |
Character |
Select the units of measure for the random variable. |
This field is optional. |
Value |
Numeric |
Select the field that contains the value you want to analyze. |
This is a required field. |
Copyright © 2018 General Electric Company. All rights reserved.