The Kolmogorov-Smirnov test is a Goodness of Fit (GOF) test applied to Reliability Distribution Analyses to determine how well the data fits the analytical curve. When you create an analysis, by default, the fit method is set to Least Squares.
After the analysis is created, you can modify the fit method to one of the following:
You can change the fit method in the Analysis Summary workspace or after selecting any of the plot tabs in the left pane.
Steps
Access a Reliability Distribution Analysis for which you want to modify the fit method.
If you want to change the fit method from the Analysis Summary workspace:
In the bottom section, select Distribution Options, and then select
The Fit Method list is enabled.
From the Fit Method list, select the desired fit method, and then select
The analysis is recalculated based on the selected fit method.
-or-
If you want to change the fit method after selecting one of the plot tabs (e.g., Probability Plot tab):
In the left pane, select the Probability Plot tab.
The Probability Plot appears in the workspace.
In the upper-right corner of the workspace, select Distribution Options, and then select Fit Method.
The Select Fit Method window appears.
Select the desired fit method, and then select OK.
The analysis is recalculated based on the selected fit method.
Copyright © 2018 General Electric Company. All rights reserved.