The Kolmogorov-Smirnov test is a Goodness of Fit (GOF) test applied to a Probability Distribution Analysis to determine how well the data fits the analytical curve. When you create an analysis, the fit method is set to Least Squares by default.
After the analysis is created, you can modify the fit method to one of the following:
You can change the fit method from the Analysis Summary workspace or from any of the plot tabs in the left pane.
Steps
If you want to change the Fit Method from the Analysis Summary workspace:
In the bottom section, select Distribution Options, and then select
The Fit Method field is enabled.
In the Fit Method box, select the desired Fit Method, and then select
The analysis is recalculated based on the selected Fit Method.
-or-
If you want to change the Fit Method from one of the plot tabs (e.g., Probability Plot tab):
In the left pane, select the Probability Plot tab.
The Probability Plot appears in the workspace.
Note: You can also change the Fit Method via the PDF Plot or CDF Plot tabs.
In the upper-right corner of the workspace, select Distribution Options, and then select Fit Method.
The Edit Fit Method window appears.
Select the desired Fit Method, and then select OK.
The analysis is recalculated based on the selected Fit Method.
Copyright © 2018 General Electric Company. All rights reserved.