You can access the source data only if the analysis is based on a query or a dataset.
Steps
In the left pane, select the Probability Plot tab.
The Probability Plot appears in the workspace.
Note: You can also view data for a plot via the Failure Rate Plot, PDF Plot, CDF Plot, or Failure Probability.
In the upper-right corner of the workspace, select Analysis Data, and then select Go To Source.
The fields on the page that appears display the analysis data associated with the selected Reliability Distribution Analysis and correspond to values that were used to create the analysis.
For an analysis based on a dataset, the information stored in the dataset appears.
For an analysis based on manually-entered data, you will receive the following error message:
There is no source data to view since the analysis is based on manually entered data.
To view data for an analysis based on manually-entered data, you can access the Reliability Distribution window.
Copyright © 2018 General Electric Company. All rights reserved.