This topic assumes that you have an established analysis with at least one Recommended Action in a Pending state.
Next to one or more Recommended Actions to which you want to modify the state assignment, select the check box.
The selected Recommended Actions are highlighted.
In the Recommended Actions pane heading, select
You can send an RBI Recommendation for approval for implementation only if ASM integration is disabled for RBI.
Using the baseline Action Management implementation, an RCM FMEA Recommendation record can be approved from the Pending state.
An RCM FMEA Recommendation record can be rejected from the Pending state.
A message appears, confirming that the selected Recommended Actions have transitioned.
Note: If you have more than one Recommended Action selected, you can also Consolidate and Supersede Recommended Actions; however, these steps are documented in a separate set of procedures.
Copyright © 2018 General Electric Company. All rights reserved.