This topic provides an alphabetical list and description of the fields that exist for the RCM Functional Failure family and appear on its datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Functional Failure ID |
Character |
The ID of the functional failure. |
Generated automatically by the system. Cannot be modified. |
Functional Failure Long Description | Text | Description of the functional failure. | You can enter a description manually. |
Functional Failure Name | Character | The name of the functional failure. | This is a required field. |
Copyright © 2018 General Electric Company. All rights reserved.