RCM FMEA Asset Records

This topic provides an alphabetical list and description of the fields that exist for the RCM FMEA Asset family and appear on its datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Asset Description Text Description of the asset. You can enter a description manually.
Asset ID Character The original Equipment ID for the asset. Populated automatically when you select an asset from the Asset Finder. This is a required field.
Asset Type List The type of asset. Generated automatically by the system. Can be modified, if needed. This is a required field.
Purpose Statement Text Purpose of the asset. You can enter a description manually.

RCM Asset ID

Character

The ID for the asset specific to the RCM module.

Generated automatically by the system. Cannot be modified.

Copyright © 2018 General Electric Company. All rights reserved.