RCM FMEA Analysis Records

This topic provides an alphabetical list and description of the fields that exist for the RCM FMEA Analysis family and appear on its datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Analysis Identification
Analysis End Date Date/Time The end date for the analysis. You can use the Calendar feature to select the date on which the analysis should end.

Analysis ID

Character

The ID of the analysis.

Generated automatically by the system. Cannot be modified.

Analysis Long Description Text A more detailed description of the analysis. You can enter a description manually.
Analysis Re-Evaluation Date Date/Time The date scheduled between the start and end dates to re-evaluate analysis parameters. This date cannot be before the Analysis Start Date.
Analysis Short Description Text A brief description of the analysis. This is a required field.
Analysis Start Date Date/Time The start date for the analysis. You can use the Calendar feature to select the date on which the analysis should begin.
Analysis Type List The type of analysis. Generated automatically by the system. Cannot be modified.
System Definition
System Boundary Description Text Details for the system boundary. You can enter a description manually.
System Criticality Character The level of criticality for the system being analyzed. This value is based on criticality evaluation outside of GE Digital APM, and therefore must be entered manually.
System Criticality Basis List The criticality basis for a system.

This field will contain one of the following values:

  • Calculated
  • Economic Analysis
  • Safety and Health Analysis
  • System Criticality Analysis
  • System Reliability Analysis
System ID Character The ID for the system. Enter a value manually in the text box.
System Long Description Text Details for the system. You can enter a description manually.
System Name Character The name of the system. Enter a value manually in the text box.
System Notes Text Any notes necessary for the system. You can enter your notes manually.
System Primary Drawing Number Numeric The number that references a drawing or diagram of the system. This value is based on an indexing system outside of GE Digital APM, and therefore must be entered manually.

Copyright © 2018 General Electric Company. All rights reserved.