On the left navigation menu, select Strategy, and then select Reliability Centered Maintenance (RCM).
The RCM Overview page appears, displaying the following tabs:
Analyses: All analyses in the module.
Risks: All the failure modes and effects associated with the analyses in the module.
Recommended Actions: All the recommendations associated with the analyses in the module.
Templates: All templates in the module.
The page contains the following charts:
Analyses by State: Plots the number of analyses in each state.
Risks Without Recommended Actions: Plots the number of failure effects in analyses with and without associated recommended actions.
Recommended Actions by Type: Plots the number of recommended actions of each type in all the analyses.
Recommended Actions by State: Plots the number of recommended actions in each state in all the analyses.
You can select in the upper-left corner of the page to filter the information displayed on the Reliability Centered Maintenance Overview page to a specific time range or asset. When you filter by an asset, the page displays information for the selected asset and the assets under it in the hierarchy. The Home level includes information not related to an asset or related to an asset not in the Asset Hierarchy.