Example of a Concurrent Quantity-Based Plan

This topic includes an example of a concurrent quantity-based Production Plan.

Note: The information contained in these topics assumes that you are the user who will be performing the associated step in creating a Production Plan and that all PLA administrative tasks have been completed.

The following image shows a concurrent quantity-based Production Plan.

Concurrent Quantity-Based Plan Example

The data used in each of the sections is listed in tables. In the tables, we list only the fields that contain a value. The information in these tables is provided for your reference.

Production Profile Data

The example assumes that the PLA Administrator has added the following two Production Profiles to the Production Unit for which you want to create a concurrent quantity-based Production Plan:

Field Value
Product 1
Product Diesel
Product UOM Barrels
Production Rate UOM Day
Standard Batch Size 23,000
Standard Batch Cycle Time 1
Max Sustained Capacity Rate 23,000
Product 2
Product Gasoline
Product UOM Barrels
Production Rate UOM Day
Standard Batch Size 103,700
Standard Batch Cycle Time 1
Max Sustained Capacity Rate 103,700

Production Summary

The example of a concurrent quantity-based Production Plan assumes that your Production Plan meets the following criteria:

Criteria Data Used in This Example
How Much

Two Products:

  • Diesel - 380,708 Barrels
  • Gasoline - 1,696,946 Barrels
When April 1, 2017 through April 18, 20167
During Which Hours

Monday through Friday, 24 hours per day, two shifts:

  • 7:00 A.M. to 7:00 P.M.
  • 7:00 P.M. to 7:00 A.M.
How Often You Enter Data Per Day
Production Model Concurrent

Copyright © 2018 General Electric Company. All rights reserved.