This topic includes an example of a concurrent time-based Production Plan.
Note: The information contained in these topics assumes that you are the user who will be performing the associated step in creating a Production Plan and that all PLA administrative tasks have been completed.
The following image shows a concurrent time-based Production Plan.
The data used in this example is listed in tables. In the tables, we list only the fields that contain a value. The information in tables is provided for your reference.
Production Profile Data
The example assumes that the PLA Administrator has added the following two Production Profiles to the Production Unit for which you want to create a concurrent time-based Production Plan:
Field | Value |
---|---|
Product 1 | |
Product | Diesel |
Product UOM | Barrels |
Production Rate UOM | Day |
Standard Batch Size | 23,000 |
Standard Batch Cycle Time | 1 |
Max Sustained Capacity Rate | 23,000 |
Product 2 | |
Product | Gasoline |
Product UOM | Barrels |
Production Rate UOM | Day |
Standard Batch Size | 103,700 |
Standard Batch Cycle Time | 1 |
Max Sustained Capacity Rate | 103,700 |
Production Summary
The example of a concurrent time-based Production Plan assumes that your Production Plan meets the following criteria:
Criteria | Data Used in This Example |
---|---|
How Much |
Two Products:
|
When | July 1, 2016 through July 31, 2016 |
During Which Hours |
Monday through Friday, 24 hours per day, two shifts:
|
How Often You Enter Data | Per Day |
Production Model | Concurrent |
Copyright © 2018 General Electric Company. All rights reserved.