The value in the Unaccounted Loss column is not stored in the Production Data and is for display purposes only. The number that appears in each cell in this column is calculated using the following equation:
Unaccounted Loss = Short Range Plan - Losses - Actual
Where Short Range Plan, Losses, and Actual are displayed in the same row as the Unaccounted Loss value.
Note: The calculated unaccounted loss is displayed using the number of decimal places defined for the Display Precision setting, regardless of the number of decimal places in the underlying Short Range, Losses, and Actual values.
Assume that the following values appear in a single row on the Production Data workspace:
In this case, the value in the Unaccounted Loss column in that row will be calculated using the following equation:
Unaccounted Loss = 5,000 - 0 - 3,000
Unaccounted Loss = 2,000
Copyright © 2018 General Electric Company. All rights reserved.