The Production Plans section appears, displaying a list of Production Plans available in the database.
In the row containing the Production Plan whose details you want to view, in the Plan ID column, select the link to access the details of the Production Plan.
The Plan Details workspace appears, displaying the details of the selected plan.
The Plan Details workspace contains the following items:
Start Time: The start time of the production plan. This value is read-only.
End Time: The end time of the production plan. If this is a time-based plan, you specified this value manually in the Production Plan Builder. Alternatively, if this is a quantity-based plan, this value is determined automatically based upon the product quantity and start time that you specified. This value is read-only.
Plan Basis: The type of plan: Time-based or Quantity-based.
Production Model: The order in which the products will be produced: Concurrent or Sequential.
Data Entry Type: How often you plan to enter production data and losses.
Upper Grid: In the Plan Details workspace, each row in the upper grid represents a separate product that is being produced during the plan. All values in the grid are read-only. The grid contains the following columns:
Product Name: The name of the product.
Quantity: The amount of product that should be produced during the entire plan. If this is a time-based plan, this value is determined automatically based upon the start and end times that you specified in the Production Plan Builder and the batch production values that you specified in the associated Production Profile. Alternatively, if this is a quantity-based plan, you specified this value manually in the Production Plan Builder.
UOM: The unit of measure that is associated with the product.
Sequence: The order in which the product will be produced during the Production plan (represented by a number 1 through n).
Note: The Sequence column is displayed only for the Sequential Production Model.
Start Time: The time at which that product will start being produced. If multiple products are being produced, the start time for each product is determined based upon your production model selection in the Production Plan Builder. For example, if multiple products are being produced sequentially, for each product after the first one, production will start after production ends for the previous product.
End Time: The time at which that product will stop being produced.
Lower Grid: In the Plan Details workspace, each row in the lower grid represents a separate period in the plan (e.g., a separate day or a separate shift within the same day). The grid contains the following columns:
Start Time: The start time of the period.
End Time: The end time of the period.
<Product Name (<UOM>)>: The planned production amount for that period. You can modify the value as long as it does not exceed the maximum demonstrated capacity that is defined in the associated Production Profile.
You can modify values in the Plan Details section by selecting the value that you want to modify. Doing so will update the value in the Quantity column in the Products section and the plan start and end time above the Products section.