Implement an EAM Maintenance Plan

In the Approved Actions section, you can implement a maintenance plan to create an implementation in the EAM system for the selected Actions.

Steps

  1. Access the Approved Actions section.

  2. In the Approved Actions workspace, select the check box in each row containing an action that you want to include in the maintenance plan.

    IMPORTANT: The maximum number of records that you can selected for one implementation is 250.

    The action(s) are highlighted.

  3. In the workspace, select Implement, and then select EAM Maintenance Plan.

    The Implement as EAM Maintenance Plan window appears.

  4. Select Send.

    A message appears, confirming that the maintenance plan has been implemented successfully.

Results

Copyright © 2018 General Electric Company. All rights reserved.