Select Edit Schedule for each of the following to determine the data collection schedule for each item in the Scheduling Settings section:
AMS Asset Schedule
AMS Asset Alert Schedule
AMS Asset Event Schedule
IMPORTANT: To ensure that the data collection schedule is executed, each occurrence should be at a different time. If schedules are at the exact same time, the collection process will fail.
In the Edit Schedule window, select either the One Time or Recurrence box.
In the Time Zone section, use the drop-down to select the appropriate time zone.
In the Start section, select to schedule the start date and time.
In the Every section, enter the numeric value indicating how often you want the generation to occur and select the appropriate interval unit (i.e., minutes, hours, years, etc).
In the Every section, select one of the following:
From start time: To start the recurrence from the previously selected start time.
After last occurrence: To begin the generation after the last time the job ran.
In the End box, based on when you want the recurrence to end, use the drop-down to select one of the following:
Never: The recurrence will not end.
After: To enter a number of occurrences after which the generation will end.
Time & Date: To use the calendar to select a time and date when the generation will end.
Select OK.
In the AMS Asset Event History row, enter the time interval, and then use the drop-down to select the unit of time.