If the default labels Risk Of, Mitigated By, Unmitigated Risk Rank, and Mitigated Risk Rank that appear on the left side of the Risk Assessment window are not suitable for your organization and terminology, you can modify the labels using the Risk Matrix record.
Note: When you modify a label, the new label will be used everywhere that the Risk Matrix record is used to display the Risk Assessment window. For example, if an Asset Strategy and an RCM Analysis use the same Risk Matrix, if you modify the labels in that Risk Matrix record, the new labels will be displayed when you access the Risk Assessment interface from any of the following items:
Steps
In the Appearance section, in the following boxes, type the new titles:
Unmitigated Risk Label: The label of section that displays the name of the risk. This will be used in place of Risk Of.
Mitigation Label: The label of the section that displays the name of the item that is mitigating the risk. This will be used in place of Mitigated By.
Unmitigated Risk Rank: The label of the section that displays the unmitigated risk rank. This will be used in place of Unmitigated Risk Rank.
Mitigated Risk Rank: The label of the section that displays the mitigated risk rank. This will be used in place of Mitigated Risk Rank.
Note: The default titles are not displayed on the datasheet. If the text boxes are empty, it indicates that the default titles are being used.
Select
Your changes are saved. The next time you view the Risk Assessment window from any item that uses this Risk Matrix (e.g., an Asset Strategy or RCM Analysis), the new titles will appear.
Copyright © 2018 General Electric Company. All rights reserved.