Determine Logging Level

You can set the logging level that will determine the logging messages included in the Data Loader log file.

Steps

  1. Access the APM Connect page, and then select Data Loaders settings.

    The Data Loaders Settings workspace appears.

  2. In the Logging Level box, use the drop-down to select one of the following logging levels:

    Notes:
    • Logging levels are hierarchical. For example, if you select Info, you will see all warnings and errors. If you select Error, you will only see errors.
    • If you are loading a large amount of data, you should use logging level Warn or Error to improve performance, unless debugging a problem.
  3. Select Save.

    The record is saved.

Results

Copyright © 2018 General Electric Company. All rights reserved.