Define a Template for Displaying Risk Values

If you have decided to display custom values in the Risk Matrix, you can create a template that will determine how values will be displayed in individual cells and on the tab labels.

For example, suppose your custom aliases appear in the Risk Matrix like this:

You can see that the risk value in each cell is a combination of the row alias and column alias, without a delimiter. You can also see that the selected risk value is reflected on the tab label. For instance, at the intersection of the Probable E row and the Very Low 1 column, you see the value E1, which is also displayed on the tab label.

You could change this so that the risk values use a delimiter, such as a dash, so you would see E-1 instead of E1.

Steps

  1. Access the Risk Matrix record for the Risk Matrix for which you want to specify how risk values will be displayed.
  2. On the Risk Matrix Layout datasheet, make sure the Use Maximum Risk Rank and Use Aliases? boxes are checked.
  3. In the Alias Format Mask box, enter a formula that represents the format in which you want risk values to be displayed, using any combination of the following parameters, with or without delimiters:

    For example, suppose you want risk values to be displayed using the format <row alias> - <column alias>. In other words, if the row alias is E and the column alias is 1, you want the risk value will be displayed as E-1. In this case, you would type the following formula in the Alias Format Mask box: {r}-{c}

  4. Select .

    The template has been defined.

Copyright © 2018 General Electric Company. All rights reserved.