About Risk Threshold Records

Each Risk Matrix is linked to multiple Risk Threshold records, where each Risk Threshold record corresponds to a range of values that are represented with the same color in the matrix, as well as the risk threshold value that appears when you pause on a cell in the matrix.

When you select a tab on the Risk Matrix, the cells in the matrix are shaded according to the value in that cell and where it falls within the ranges as they are defined in the Risk Threshold records. For example, in the following image, you can see that the cells contain in the number 0.1 and 0.01 are colored LightGreen. If you pause on the cell, the tooltip says Low.

The following Risk Threshold records are provided in the baseline GE Digital APM database to support the baseline Risk Matrix.

From the values in these records, we can determine that the following criteria will be applied to numbers that appear on the baseline Risk Matrix:

Copyright © 2018 General Electric Company. All rights reserved.