Uninstall the Barcode Add-on on Windows Mobile Device

Steps

  1. On the Windows Start menu, select Programs.

    The Programs screen appears.

  2. Select APM Mobile Framework.

    The Meridium APM Mobile Framework screen appears.

  3. Select Applications.

    The Add/Remove Applications screen appears. This following image shows an example of the Add/Remove Applications screen.

  4. In the list of available applications, to the right of Barcode, select Uninstall.

    The Uninstall screen appears, prompting you to enter your username and password.

  5. In the User ID box, enter your username.

    The Uninstall button is enabled.

  6. In the Password box, enter your password.

    Note: If the credentials that you enter are not associated with a Security User who is a Super User or member of the MI Operator Rounds Administrator Security Group, a message will appear, indicating that you do not have the privileges required to uninstall the application.

  7. Select Uninstall.

    The uninstallation process begins. The APM Mobile Framework closes, and the Barcode add-on is uninstalled.

Copyright © 2018 General Electric Company. All rights reserved.