Steps
On the Windows Start menu, select Programs.
The Programs screen appears.
Select APM Mobile Framework.
The Meridium APM Mobile Framework screen appears.
Select Applications.
The Add/Remove Applications screen appears.
In the list of applications, select the Install button that appears to the right of RFID.
A message appears, asking if you want to install the RFID add-on.
Select Yes.
The installation process begins. During this process, the APM Mobile Framework closes, and the RFID add-on is installed.
Note: After the installation process is complete, the APM Mobile Framework reopens automatically, and the APM Mobile Framework screen appears.
Copyright © 2018 General Electric Company. All rights reserved.