Install Microsoft Sync Services for ADO.NET on Windows Mobile Device

Steps

  1. On the Windows Mobile handheld device, open Internet Explorer, and then navigate to the URL http://<machine>/MeridiumSyncService, where <machine> is the name or IP address of the server on which APM Sync Services is installed.

    You are redirected automatically to one of the following URLs, and then a download screen appears:

  2. If the device is running Windows Mobile 2003, select PPC2003\SYNCSERVICES.WCE.CAB.

    or

    If the device is running Windows Mobile 5.0 or later, select WCE500\SQLCE.WCE5.ARMV4i.CAB.

    A message appears, asking if you really want to download the file.

  3. Select Yes.

    The file is downloaded, and the Microsoft Sync Services for ADO.NET is installed. When the installation is complete, a message will appear, indicating that the installation is successful.

Copyright © 2018 General Electric Company. All rights reserved.