Install Microsoft SQL CE on Windows Mobile Device

Steps

  1. On the Windows Mobile handheld device, open Internet Explorer, and then navigate to the URL http://<machine>/MeridiumSyncService, where <machine> is the name or IP address of the server on which APM Sync Services is installed.

    You are redirected automatically to one of the following URLs, and then a download screen appears:

  2. If the device is running Windows Mobile 2003, select PPC2003\SQLCE.PPC.ARM4.CAB.

    or

    If the device is running Windows Mobile 5.0 or later, select WCE500\SQLCE.WCE5.ARMV4i.CAB.

    A message appears, asking if you really want to download the file.

  3. Select Yes.

    The file is downloaded, and the Microsoft SQL CE is installed. When the installation is complete, a message will appear, indicating that the installation is successful.

Copyright © 2018 General Electric Company. All rights reserved.