Install the Barcode Add-on on Windows Mobile Device

Steps

  1. On the Windows Start menu, select Programs.

    The Programs window appears.

  2. Select APM Mobile Framework.

    The Meridium APM Mobile Framework window appears.

  3. Select Applications.

    The Add/Remove Applications window appears.

  4. In the list of available applications, select the Installbutton that appears to the right of Barcode.

    A message appears, asking if you want to install the Barcode add-on.

  5. Select Yes.

    The installation process begins. The APM Mobile Framework closes, and the Barcode add-on is installed.

    Note: After the installation is complete, the APM Mobile Framework will reopen automatically, and the APM Mobile Framework screen appears and you can enable Barcode scanning.

Copyright © 2018 General Electric Company. All rights reserved.