GE Digital APM provides the following baseline Security Groups for use with Thickness Monitoring and provides baseline family-level privileges for these groups:
Access to certain functions in GE Digital APM is determined by membership in these Security Groups. Note that in addition to the baseline family-level privileges that exist for these Security Groups, users will also need at least View privileges for all customer-defined predecessor or successor families that participate in the Thickness Monitoring relationships. Keep in mind that:
The following table summarizes the functional privileges associated with each group.
Function | Can be done by members of the MI Thickness Monitoring Administrator Group? | Can be done by members of the MI Thickness Monitoring Inspector Group? | Can be done by members of the MI Thickness Monitoring User Group? |
---|---|---|---|
Configure Global Preferences | Yes | No | No |
Configure Family Preferences | Yes | No | No |
Use the T-Min Calculator | No | Yes | No |
Archive Corrosion Rates | No | Yes | No |
Reset the Maximum Historical Corrosion Rate |
Yes |
No | No |
Exclude TMLs | No | Yes | No |
Renew TMLs | No | Yes | No |
Reset User Preferences | Yes | No | No |
Copyright © 2018 General Electric Company. All rights reserved.