Deploy Cognitive Analytics for the First Time

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic GE Digital APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Note: If you are deploying this module in APM Now, before you begin completing these tasks, review the system requirements for this module to identify the supported features for this module in APM Now. Unless noted, all deployment tasks in the following table are applicable for the deployment of this module in APM Now.

Step Task Notes
1 Review the Cognitive Analytics data model to determine which relationship definitions you will need to modify to include your custom equipment and location families or to store your classified data in custom families. Via Configuration Manager, modify any relationship definitions as needed.

This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families or if you store classified data in families other than the baseline Classified Equipment Standard and Classified Work History Standard families.

2

Assign Security Users to one or more of the Cognitive Analytics Security Groups or Roles.

This step is required.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.