After installing the Meridium Device Service, you can make changes to certain configuration settings. The Meridium Device Service is designed to function without additional configuration. Generally, you will only make changes to the configuration if you need to increase the client timeout period, or change the port the service uses (by default, port 2014).
Steps
In the text editor, navigate to the appSettings section (lines 24 to 28).
On line 25, edit the port number used by the service.
Note: The datalogger settings in Thickness Monitoring must be modified so that the port number matches the one defined in this step.
Save the file, and then close the text editor.
Restart the Meridium Device Service.
The Meridium Device Service configuration settings are updated.
Copyright © 2018 General Electric Company. All rights reserved.