About Configuring Policy Execution

Policy designers can configure a policy to be executed on a schedule or automatically when records or reading values associated with the policy are updated. This topic describes the ways that the items configured in the first-time deployment workflow facilitate each type of policy execution.

Note: Only the active instances of active policies are executed.

Automatic Execution

When records or reading values associated with the policy are updated, the GE Digital APM Server adds messages to the policy trigger queue. The Policy Trigger Service monitors the trigger queue. When it receives a message, it determines which policy instances should be executed for the message, and then it sends corresponding messages to an appropriate policy execution queue. Finally, the corresponding Policy Execution Service executes the policies associated with the records or reading values that were updated.

Scheduled Execution

When a policy is due, the scheduled job adds a message to the policy trigger queue. The Policy Trigger Service monitors the trigger queue and sends messages to the appropriate policy execution queue. Finally, the corresponding Policy Execution Service executes the policies that are due.

Copyright © 2018 General Electric Company. All rights reserved.