Scenario records are used to determine values in a scenario and store information about the fields in a scenario. This topic provides an alphabetical list and description of the fields that exist for the Scenario family. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Analysis Key | Numeric | The numeric key associated with the Analysis. | System Generated field that is hidden by default. |
Description |
Text |
The details of the scenario. |
Text entered in the Description field to describe a scenario. |
Internal Rate of Return (IRR) | Numeric | The discount rate used to make the net present value equal 0. | This field is automatically populated. |
Is Template |
Logical |
Identifies whether or not a scenario has been saved as a template. |
This field is required. |
Measurement Frequency |
Character |
A value describing the unit of rate capacity. This value is used in conjunction with Monetary Value and Unit of Measure. |
The Rate of Measure must be one of the following:
This field is required. |
Measurement Unit | Character |
A value that defines the unit of measure (e.g. gallons, miles, pounds) that is applicable in the Operating Profile. |
This value is used in conjunction with Monetary Value and Rate of Measure This field is required. |
Name |
Character |
The value used to identify the scenario. |
This field is required. |
Net Present Value(NPV) | Numeric | The sum of the present values of incoming and outgoing cash flows over an analysis period. | This field is not required. |
Rate Capacity | Numeric | A value describing the maximum rate of measurement (e.g. 5000 gallons/Year). | This field is required. |
Total Capital Cost | Numeric | The sum of all Capital Costs in a scenario. |
This field is automatically populated. This field is required. |
Total Cost of Ownership | Numeric | The sum of all costs required for the ownership of an asset in a scenario. |
This field is automatically populated. This field is not required. |
Total Operational Cost | Numeric | The sum of all costs needed for asset operations in a scenario. |
This field is automatically populated. This field is required. |
Value of Unit | Numeric | A monetary value per unit measurement (e.g. $1000/gallon). |
This value is used in conjunction with Rate of Measure and Unit of Measure.
This field is required. |
Copyright © 2018 General Electric Company. All rights reserved.