Resource Records

Resource records store information about the resources used in scenarios. This topic provides an alphabetical list and description of the fields that exist for the Resource family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Description

Text

The details of the resource.

Text entered in the Description field to describe the resource.

Name

Character

The value used to identify the resource.

This field is required.

Type

Character

The selection of the type of resource.

The Type must be one of the following values:

  • Labor
  • Part

 

This field is required.

Unit

Character

The selection of the resource unit.

The Unit field is entered.

This field is required.

Unit Cost

Numeric

The cost of the unit resource.

This field is required.

Copyright © 2018 General Electric Company. All rights reserved.