Period Records

Period records store information about the periods in scenarios. This topic provides an alphabetical list and description of the fields that exist for the Period family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Name Character The value used to identify the period. This field is required.
Scenario Key Numeric The Entity Key of the scenario record. System Generated field that is hidden by default.
Sequence Numeric A number indicating the order of the period.

This value begins with 0.

This field is required.

Copyright © 2018 General Electric Company. All rights reserved.